DIO.POWERWEN

Description

DIO.POWERGWEN enables/disables Warning 2011 “No Power on 24V IO Rail”.

Versions

Action Version Notes
Implemented 02-14-03-000  

General Information

Type Read/Write
Units N/A
Range 0 (disabled, 1 (enabled)
Default Value 1
Data Type Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported